Open Source RTOS Comes to IoT Lynnette Reese
The complexity of IoT extends beyond simple projects. If you were to take all the useful data and manipulate it, you could find patterns that point to changes that can increase productivity, reduce wait times, or point to trends that help improve processes or locate potential failures.

Electronics’ Wizardry: An Arduino Compatible Human-Machine Interface To Win Friends And Impress People Mike Parks
Makers and engineers now have a ridiculously easy way to add a high quality touchscreen display to the Arduino UNO without a lot of fuss. It’s called the CleO35 and seems ideal for projects that need a simple yet elegant Human-Machine Interface (HMI). That’s nerd speak for the barrier between the human user and the digital device. The CleO35 was first introduced on Indiegogo, a crowdfunding site, by FTDI Chip.

Xpress Your Designs to the World! Microchip MPLAB® Xpress Development Board Paul Golata
I have recently incorporated the Fractal Audio AX8 as an all-in-one Amp Modeler + Multi-Effects Pedalboard Processor in lieu of my traditional amplifier. And as a base rock-n-roll patch, I have programmed the Trainwreck Express.

The Open Yocto Project Makes Embedded Linux Simple Daniel Hankewycz
With the decrease in cost of microprocessors and ARM cores, embedded Linux systems have become more accessible to the general public. Sure, it’s easy to just slap an Arduino on your project and call it done, but what if you want to go one step further and actually make your own Linux solution? The development team behind the open source Yocto Project have made compiling a custom Linux image simpler than ever.

Tools Bridge The Chasm Between Hardware and Software Arden Henderson
Suppose some hardware folks somewhere invent a machine made of hardware that does something when it carries out a series of instructions. The instructions will be in a language the machine understands. Instructions for the machine are written in the "machine language" of the hardware, sometimes called "machine code." The machine language is the final low-level language in the journey from high level language to low-level language, resulting in correct instructions that do something useful; it is the language the machine understands.

All Authors

Show More Show More
View Blogs by Date