Deploying Edge-Based AI Using the KRIA SoM
Image Source:
Itsanan/Shutterstock.com
By Adam Taylor for Mouser Electronics
Published August 27, 2021
Introduction
Production lines are fast-paced environments. The ability to detect manufacturing or packaging defects before
shipping is critical to improving delivery and customer satisfaction. However, automated inspection equipment
needs to process and make decisions without slowing the production line. This is where equipment such as the Kria K26 System on Module (SoM) from
Xilinx can help.
The Kria K26 SoM (Figure 1) allows developers to leverage the parallel nature of programmable
logic combined with high-performance Arm processor cores. What is exciting about the Kria SoM is that for the
first time, Xilinx provides the heterogeneous SoC and the necessary supporting infrastructure for the SoC
(XCK26), such as 4GB DDR4 Memory, 16GB eMMC, 512Mb QSPI, TPM Security module, and the necessary power
infrastructure.
Figure 1: Kria SoM
To make it easy to interface with your application, dual 240-pin connectors are provided that break out 245 IO.
Xilinx also offers the Kria KV260 Vision AI Starter Kit to enable developers to get started and hit the ground
running. The kit provides developers with a carrier card for the SoM, which offers the following interfaces:
- 3 MIPI Interfaces
- USB
- HDMI
- Display Port
- 1 GB Ethernet
- Pmod
This starter kit also comes with a range of applications that show how easy it is to get started developing
vision-based artificial intelligence applications. This makes the Kria Vision AI Starter Kit perfect for the
applications where fast image processing is required, such as detecting whether or not a label has been
correctly applied to a shipping box on the production line.
Manufacturing Application Use Case
Let’s look deeper at how the Kria KV260 Vision Starter Kit can be used for a manufacturing application.
Creating a manufacturing application is not necessarily going to require any programmable logic design. However,
it will require software development and the ability to train and compile a new machine-learning model using
Vitis AI from Xilinx. The first step is installing and configuring Vitis AI for use.
Bill of materials
- Kria KV260 Vision AI Starter Kit
Creating a Virtual Machine
Running Vitis AI requires either a Native Linux machine or a Linux Virtual Machine running one of the supported
Linux Distributions.
Creating a Virtual machine that can run Vitis AI is simple. First, download the Oracle Virtual
Box.
Once the virtual box is installed, download the Ubuntu Linux disk image that can be used to install Linux on the
virtual machine. The version of Ubuntu used for this project is Ubuntu-18.04.4 Desktop-amd64.iso available here.
We are now able to build the virtual machine. The first step is in the virtual box manager to click on
New.
This will present a dialog that enables the creation of the new VM (Figure 2). Enter a name for
the VM and select the type as Linux and version as 64-bit Linux. We can also decide how much system memory is
needed to share with the virtual machine (Figure 3).
Figure 2: Creating the VM
Click on the create button, and the settings for the virtual hard disk will be presented. Select 512GB, which
allows the physical storage to be dynamically allocated. The Virtual Hard Disk size will expand to 512GB as disk
usage increases. This project was developed using an external solid-state USB C drive to store the Virtual Hard
Disk to ensure the space available.
Figure 3: Setting the memory requirements
With the VM configured, the next step is to install the operating system. With the newly created VM selected,
click on the start button to fire up the VM 9 (Figure 4).
Figure 4: Starting the VM
As the VM starts, it will ask for the Ubuntu ISO downloaded previously (Figure 5).
Figure 5: Installing the installation disk
The next steps are to install the Ubuntu operating system on the virtual hard disk. Select install Ubuntu
(Figure 6).
Figure 6: Installing Ubuntu
Select the options as to location and configuration of Ubuntu. Select the keyboard configuration (Figure
7).
Figure 7: Selecting localization
Select minimal installation (Figure 8) as we will not use office software, media players, or
games.
Figure 8: Select Minimal Installation
Allow the installation process to erase the disk and install Ubuntu (Figure 9).
Figure 9: Erasing the disk
Click continue to proceed with the changes (Figure 10).
Figure 10: Enable Disk Overwrite
Select your location and time zone (Figure 11).
Figure 11: Setting the time zone
Finally, enter the Ubuntu computer name, username, and password (Figure 12).
Figure 12: Setting the account name and password
Finally, once the installation is completed, restart the virtual machine (Figure 13).
Figure 13: Restart the machine
Once the VM restarts, log in and start installing Vitis AI (Figure 14).
Figure 14: Logging in
Installing Vitis and Vitis AI
With the Virtual Machine running Linux, our next step is to install both Vitis and Vitis AI. You will need a
Xilinx user account to install Vitis, which can be created as part of the download process. As Vitis is the
longer of the two installs, we will start with that first.
Go to the Xilinx
downloads page and select the Linux Self Extracting Web Installer (Figure 15).
Figure 15: Xilinx Linux Installer
With the web installer downloaded, navigate to the download location, select the application, and right-click it
to change its permissions to enable it to be executed as an application (Figure 16).
Figure 16: Setting the correct permissions
We can now use a terminal window to install Vitis. This might take time depending upon the capabilities of your
VM and internet connection.
Use sudo to install the tool with the command (Figure 17).
sudo ./Xilinx_Unified_2020.2_1118_1232_Lin64.bin
Figure 17: Running the installer
This will start the Vitis Installer (Figure 18).
Figure 18: Starting the installer
Sign in to your account (Figure 19).
Figure 19: Signing into your Xilinx account
Select Vitis as the target application. This includes Vivado (Figure 20).
Figure 20: Installing Vitis with Vivado
To reduce the installation size, uncheck all devices but the SoCs (Figure 21).
Figure 21: Minimizing the installation footprint
Agree to the terms and conditions (Figure 22).
Figure 22: Agreeing to Terms and Conditions
Select the installation directory. I suggest leaving it as default (Figure 23).
Figure 23: Selecting the installation location
On the installation summary, select install and wait (Figure 24).
Figure 24: Completing installation
Once the installation is complete, we need to run the script below to install all the dependencies:
sudo <install_dir>/Vitis/<release>/scripts/installLibs.sh
The next step is to install Vitis AI. In this instance, we will install Vitis AI to run from the CPU and not the
GPU, which will mean slower training performance.
The first step is to install docker. This can be achieved following the instructions here. Note, it might be necessary to restart the Virtual
Machine once this has been completed.
The following steps are to install Git using the commands:
sudo apt update
sudo apt install git
Select/create a directory to install Vitis-AI clone the Vitis-AI using the command:
git clone https://github.com/Xilinx/Vitis-AI.git
Once the Vitis-AI repository has been cloned, the next step is to change the directory into it and pull the
docker image.
cd Vitis-AI
docker pull xilinx/vitis-ai:latest
This will take several minutes to download the latest Vitis-AI image from docker.
After the docker image has been pulled, we need to build the cross-compilation system. We can do this by running
the script located under Vitis-AI/setup/mpsoc/VART (Figure 25).
cd Vitis-AI/setup/mpsoc/VART
./host_cross_compiler_setup_2020.2.sh
Figure 25: Installing the SDK Path
Once the script has run, be sure to run the indicated command to enable the cross-compilation environment.
We can test if we have installed Vitis AI correctly by compiling one of the demonstration programs. In this case,
the resnet50 application provided under the demo/VART/Resnet50 directory. To build the application, use the
command:
Bash -x build.sh
Provided you see no errors reported in the terminal window and the executable appears in the directory, the Vitis
AI installation is working (Figure 26):
Figure 26: Compiling the Engine
Now we need to start developing the data set that shows the labels correctly and incorrectly applied.
Creating the Data Set
To train a neural network, we first need a data set of correct and incorrect images. To do this, several boxes
were applied with the Mouser labels both correctly and incorrectly. To have a diversity of images, both the
correct and incorrect boxes were photographed from several angles (Figures 27 and 28).
Figure 27: Correct image selection
Figure 28: Incorrect image selection
The images were collated into two directories - one for the correct label and another for the incorrect label.
With the images captured, we need to train a neural network. To do this, I will use edge impulse to train the
neural network as it makes the training easy. Note that you will need to create an account for edge impulse, but
it is free.
In edge impulse, the first thing to do is create a new project (Figure 29).
Figure 29: Creating an Edge Impulse Project
Once the new project has been created, we can upload the images folders, labeled as correct and incorrect. Select
all of the files first in the correct directory and upload with the label Label_Correct. After upload of
the correct images, upload the incorrect images and label them Label_Incorrect (Figure 30).
Figure 30: Uploading the data
With the images all uploaded, the next step is to define the impulse. Select an input image width and height of
224px in each direction. Select an image input and then the Transfer Learning. Save the impulse (Figure
31).
Figure 31: Setting the impulse
We can then train the model, by generating the features and training the impulse (Figure 32).
Figure 32: Generating the features
Select the model MobileNetV2 160x160 1.0. An equivalent model is in the Xilinx Model Zoo (Figure
33).
Figure 33: Selecting the correct model
Train the model. This might take a few minutes. Once the model has been trained, go back to the overview page and
select the download transfer learning model (Figure 34).
This will include the saved model and the variables (checkpoint) in a .zip file.
Figure 34: Downloading the saved model
Quantizing and compiling the model
The next step is to quantize and compile the model using Vitis AI. In the virtual machine, we can run Vitis AI by
issuing the following command (Figure 35).
./docker_runs.sh Xilinx/vitis-ai-cpu:latest
Figure 35: Starting Vitis AI
With Vitis AI loaded, activate TensorFlow with the command (Figure 36).
conda activate vitis-ai-tensorflow
Figure 36: Vitis AI TensorFlow activation
The next step is to freeze the model that merges all the information from the checkpoint into the frozen model
file (Figure 37).
Figure 37: Compiling the frozen model
Once the model has been output as a frozen model, we can use the compiler to compile the output model so that we
can deploy it on the system.
We can learn the information of the output nodes from the YAML file contained within the Xilinx Model Zoo
(Figure 38).
Figure 38: Exploring the model
To inspect the frozen netlist, we can install Netron. It is important to understand the input and output nodes
names for the quantization process (Figure 39).
Figure 39: Installing Netron
With a quantized netlist available, we can compile the quantized netlist to a model deployed on the Kria SoM
(Figure 40).
vai_c_tensorflow -f /quantized_model.pb -a arch.json -o ./tf -n Output
Figure 40: Compiling the model
Using SCP/FTP, we can upload the compiled model to the Kria file system under:
/usr/share/vitis_ai_library/models/
With the model uploaded, we can generate a software application that can be used to test the neural network. To
do this, several correct and incorrect images are uploaded to the Kria SoM and used to test the application
(Figure 41 and 42).
Figure 41: Correctly identifying an incorrect label
Figure 42: Correctly identifying a correct label
Wrap Up
This project has shown how easily a neural network can be trained and deployed in the Kria SoM for industrial AI
/ ML applications. The potential is limitless. Future adaptations could be to update the software to utilize the
gstreamer framework and classify images live as they would be on the production line.
Author Bio
Adam Taylor is a professor of
embedded systems, engineering leader, and world-recognized expert in FPGA/System on Chip and Electronic Design.